A Complete Guide To Coaxial Connectors

Find out about coaxial connectors: what they are, what types are on the market and what they're used for.

coaxial-connector-guide-banner

What is a coaxial cable?

Coaxial or ‘coax’ cables are electrical cables created to carry high frequency, multi-megahertz electrical signals. They contain an inner conducting wire, usually copper, surrounded by a protective double insulating layer and then an outer plastic sheath, giving them a distinctive appearance.

Coaxial cables are durable, easy to install, and have a broad range of uses. Their design allows rapid signal transmission (around 10 megabits per second) with minimal electro-magnetic interference or signal loss. Coaxial cables are the default cabling choice for many low voltage consumer electronics. These include:
  • Televisions and telephones
  • Mobile phones
  • Satellite dishes
  • Broadband routers
  • Antennas
  • Radio equipment

Coaxial cables are available in a variety of types, distinguished by their ‘gauge’ and ‘impedance’. Gauge refers to the thickness of the cable and is given a given a Radio Guide or RG number, with higher numbers indicating thinner conducting cores. Impedance refers to the level of electrical resistance in the wire. Most coaxial cables have an impedance of either 75 or 50 Ohm. The former is primarily used for video signals and the latter for data.

Coaxial cables can come in many sizes, including:

The section below will give you some information about some of the most common coaxial cables available on the market. For more information regarding coaxial cables, please visit our other guide: Everything You Need To Know About Coaxial Cable.

The most common coaxial cable sizes are:

RG-6: As indicated by the low number, these cables have broad central conductors with thick insulation and specialist shielding, which allows a strong signal. The cables themselves are thin, however, making them ideal for installation in ceilings and within and along walls.

RG-11: These cables are relatively thick but as a result, more resistant to signal loss, making them a good choice for lengthier installations.

RG-59: The RG-59 resembles the RG-6 but, as suggested by the high number, it has a thin central conductor, making it best for low frequency transmission over limited distances – for example in the home.

TE-Connectivity-Male-BNC-to-Female-BNC-RG58-Coaxial-Cable-img

What is a coaxial connector?

Coaxial connectors, also known as barrel or tip connectors, are used to top and tail the cables and connect devices to external power supplies, or to connect cables to each other, while maintaining the outer interference shielding.

They are available in a multitude of different sizes to suit different cable dimensions, each of which works in combination to ensure smooth transmission of the signal.

Some include switches that allow internal batteries to be disconnected when an external power supply is connected.

Types of coaxial connectors

Coaxial cables are used for many different purposes and so the connectors are equally varied. Each type and size is carefully designed to mesh seamlessly with the host cable and function in different, sometimes quite tough conditions. They must resist such stressors as impact, pressure, high temperature and vibration.

Coaxial cables made for radio frequency (RF) transmission require special connectors that provide consistent electrical resistance at the point of connection with connected cables. This means they are somewhat delicate and can be damaged easily.

The major types of coaxial connector are:

7/16 DIN Connectors

7/16-DIN-Connectors-Male-Female-img

These are tough, threaded connectors primarily used for connecting lengths of coaxial cable within environments which are exposed to moisture.DIN stands for the Deutsches Institut für Normung – the “German Standardisation Institute”.

Commonly used in:

  • Radio base stations
  • Broadcasting equipment
ช่วงดู

BNC Connectors

BNC-Connectors-Male-Female-Img

BNC (Bayonet Neil-Concelman) connectors are a smaller variety of connector used for test instruments,radio, television and other AV equipment.

Designed for:

  • Rapid connection
  • Rapid disconnection
ช่วงดู

F Connectors

f-coaxial-connectors-male-female-img

Also known as F-type connectors,these are commonly used to conduct an electrical signal to TV sets

Can be paired with:

  • RG6 cables
  • RG59 cables
ช่วงดู

FME Connectors

fme-coaxial-connectors-male-female-img

These are miniature threaded connectors. The name itself stands for ‘For Mobile Equipment’.

Most commonly used with:

  • Mobile equipment
ช่วงดู

MBX Connectors:

MBX-coaxial-connectors-male-female-img

MBX connectors are used to make connections within radio frequency equipment.

Key features

  • Very robust
  • Offer good power handling
  • Great electrical performance
ช่วงดู

MCX Connectors

MCX-coaxial-connectors-male-female-img

MCX stands for ‘micro coaxial’, and as the name suggests, these are a smaller connector ideal for use in locations where space is limited.Like many other coaxial connectors, they are designed for easy attachment and removal.

Ideal applications:

  • TV tuner card for PC's
  • GPS systems
  • Wi-fi routers
ช่วงดู

MMBX Connectors

MMBX-coaxial-connectors-male-female-img

Similar to MBX connectors, MMBX connectors provide reliable and flexible connections within radio communications equipment even if misaligned.

Key feature:

  • Allows multiple connections between adapters
ช่วงดู

N Connectors

N-coaxial-connectors-male-female-img

Also known as ‘N-type connectors’, these medium-sized adapters boast many features, such as being waterproof.They were named after their inventor, American electrical engineer Paul Neill.

Ideal application:

  • Radio transmission equipment
ช่วงดู

OSMT Connectors

Male-Straight-Surface-Mount-50Ω-OMST-Connector-img

OSMT connectors are typically made from polymer and gold/nickel plating.

Widely used within:

  • Telecoms
  • GPS devices
  • Vehicle and consumer electronics
ช่วงดู

OSP Connectors

Male-Straight-Miniature-50Ω-Panel-Mount-OSP-Connector-img

These connectors feature a snap-on or slide mechanism for ‘mating’ (see Coaxial connector gender types below).

Used with:

  • Radio equipment
ช่วงดู

QLI Connectors

Radiall-QLISeries-50Ω-QLI-Connector-jack-img

These connectors are a variant of DIN 7/16 connectors, making use of the same bayonet locking mechanism and offering similar performance.

Key features:

  • Very tough
  • Continue performing in harsh environments
ช่วงดู

QMA Connectors

qma-coaxial-connectors-male-female-img

QMA connectors are a second variant of SMAs – the Q stands for ‘quick’, and they are designed for rapid, easy attachment and detachment without a torque spanner.QMA connectors have a robust design and are resistant to vibration, making them ideal for use in outdoor settings.

Ideal applications:

  • Radio base stations
  • Air traffic control systems
  • Transmision equipment
ช่วงดู

QN Connectors

Straight-50Ω-RF-Adapter-QN-Plug-to-Type-N-Socket-img

These are a quick-lock variant of the N-type connector and are compatible with high power cables.

Ideal for:

  • Indoor applications
  • Outdoor applications
ช่วงดู

RCA Connectors

RCA-coaxial-connectors-male-female-img

RCA stands for the Radio Corporation of America and the name paints a picture of this connector’s origins. It was devised in the 1940s for use within vinyl turntables.They are also known as cinch connectors and their plugs as ‘phono plugs’, a reference to the phonograph, one of the earliest forms of recording device.RCA connectors are still used in audio and video equipment.

Used with:

  • Camcorders
  • Video game consoles
ช่วงดู

SHV Connectors

Radiall-Straight-50Ω-Panel-Mount-SHV-Connector-img

‘Safe High Voltage’ or SHV connectors use a bayonet-locking mechanism which is similar to that used in MHV and BNC connectors.They feature a distinctive protruding insulator.

Designed for:

  • Safe use with high voltage cables
ช่วงดู

SMA Connectors

SMA-coaxial-connectors-male-female-img

SMA (Subminiature version A) connectors can often be confused with the F coax connector. However, there is a slight (2mm) difference between the two difference types.

Typically used for:

  • Walkie talkies
  • Handheld radios
  • Radio telescopes
  • Wi-fi antennas
ช่วงดู

SMB Connectors

SMB-coaxial-connectors-male-female-img

Similar to the above, Subminiature version B (SMB) connectors have an easy-to-use design.

Widely used with:

  • Telecoms equipment
  • Industrial electronics
ช่วงดู

SMC Connectors

RS-PRO-Straight-50Ω-Panel-Mount-Bulkhead-Fitting-SMC-Jack-IMG

SMC, or SubMiniature version C, are, as the name suggests, a second variation of the SMA connector. They have a screw-type interface.

Key feature:

  • Provides air-tight closure against leakage and damage.
ช่วงดู

SMP Connectors

SMP-coaxial-connectors-male-female-img

Subminiature push-on, or SMP, connectors have a snap-on interface and strong electrical performance. They are agood choice for use in more demanding environments.

Key features:

  • Very robust
  • Can withstand shock and vibration
ช่วงดู

TNC Connectors

TNC-coaxial-connectors-male-female-img

TNC (Threaded Neil-Concelman) connectors are a variation of BNC connectors designed for outdoor use.

Common uses:

  • Radio antennas
  • Mobile phone antennas
ช่วงดู

Triax Connectors

Male-Straight-Cable-Mount-Triax-Connector-img

These variants of the basic BNC connector are used, as the name suggests, with triaxial or ‘triax’ cables.They provide greater bandwidth but are more expensive.

Key features:

  • An additional layer of insulation
  • An extra conucting sheath
ช่วงดู

Twinax Connectors

RS-PRO-Straight-100Ω-Cable-Mount-Twinax-Connector-img

Twinax connectors are a doubled variation of the BNC connector and are used to prevent signals from being mixed.hey are also known as ‘Twin BNC’ connectors.

Key features:

  • A latching mechanism
  • Crimp connectors for easy installation
  • Both male and female contact points
ช่วงดู

TV/Aerial Connectors

TV-Aerial-coaxial-connectors-male-female-img

TV/Aerial connectors are one of the most common connectors seen on the market.

Normally used with:

  • Television sets (ones which contain an aerial socket)
ช่วงดู

UFL Connectors

Radiall-Straight-Miniature-50Ω-PCB-Mount-MML-Connector-img

These connectors are built for use in tight spaces.

Ideal applications:

  • Printed circuit boards
  • Small radio frequency devices
  • Plug-in wi-fi attachments
ช่วงดู

UHF Connectors

UHF-coaxial-connectors-male-female-img

UHF stands for Ultra High Frequency, but despite the name technology has moved on since their invention and they are now primarily used with low frequency devices.

Commonly used as:

  • Video connectors for military equipment
ช่วงดู

UMCC Connectors

TE-Connectivity-Surface-Mount-UMCC-Connector-img

The ‘Ultraminiature Coax connector’ (UMCC) is used for frequency signals up to 6Ghz in extremely small scale environments – for example, laptop circuit boards and embedded circuitry.

Commonly used to:

  • Make connections to GPS
  • To connect to wi-fi antennas
ช่วงดู

How to choose your connector

When selecting a coaxial connector, you will need to know the key parameters of the cable you plan to connect. These include:

  • The voltage
  • The environment
  • The required frequency
  • Whether a male or female connection is required. ‘Male’ connector have protruding metal pins while ‘female’ connectors have a recess designed to receive the pins (see below).

Coaxial connector gender types

In electrical engineering, coaxial and other electrical cables are conventionally divided into two types: male and female. The former typically have a connecting pin or protrusion of some kind that is inserted into indentations or slots in the latter – for example, plugs and sockets (also known as ‘jacks’). Connecting a male to a female connector is referred to as ‘mating’ them.

Coaxial cable genders were designed not just to allow physical connections but also to ensure that power or signal data flows in the correct direction, from male to female connectors with matching electrical polarity, preventing interference and unsafe installations. Typically, female connectors are more resistant to damage than male ones so these tend to be placed in crucial areas with males relegated to connecting cables, which can be replaced more easily.

Note that the terms ‘male’ and ‘female’ are not universally used, especially in relation to lower voltage domestic appliances. Widely used electrical standard IEC60320 does not specify gender types for the latter.

Male coaxial connectors

Male coaxial connectors typically have a straightforward design, combining a central pin designed to fit a compatible plug on the female connector, alongside a spring-loaded electrical contact point located at the side.

Female coaxial connectors

Female coaxial connectors normally feature a metallic tube designed to precisely contain the corresponding male pin, normally called the ‘tip’. This is surrounded by an insulating layer and then an outer cylinder, typically referred to as the ‘barrel’ or ‘sleeve’. The latter functions as an electrical contact point, alongside the inner tube.

Genderless coaxial connectors

So-called ‘genderless’ coaxial connectors combine male protrusion points and female slots in the same connection point, enabling these to be connected to either male or female connectors of matching size and type. They allow cabling within complex installations to be repurposed or reconnected quickly, without awkward removal and repositioning if it needs to be connected to a different component or cable. They have a reverse electrical polarity, with a pin protruding from the female socket and slot in the male plug designed for that pin.

Genderless coaxial connectors are also known as ‘hermaphrodite’, ‘androgynous’ or ‘combination’ connecters. They are not the right choice for installations in which a carefully controlled flow of current in a single direction is required for safety or reasons of function.

FAQs

How do you connect or change a coaxial connector?

Coaxial cables and their corresponding connectors have different uses but the fundamentals of connecting or replacing them remain much the same. Here’s how to conduct this procedure:
  1. Ensure that the cable from any power sources. Electrical shocks and injuries could result from adjusting a live coaxial cable.
  2. If there is already a connector in place, remove it. It may respond to a simple twist or you may need to make use of tool, such as a construction knife or wire strippers.
  3. Prepare the coaxial cable, using that wire stripper or a similar device. Make a small incision towards the end of the cable, deep enough to expose the underlying copper, and then a second cut in the outer jacket of the cable – in both cases being careful not to cut into the underlying layers. Use these cuts as leverage to peel back the jacket and then the wire braiding beneath, going back the same length as the connector.
  4. Place the connector onto the exposed length of wire.
  5. Attach the connector to the wire by applying pressure. Use a compression tool – for example, a pair of pliers – or a more specialist crimping tool. Crimping is only a modified form of compression, so the two methods are very similar. In both cases, insert the connector which has been placed over the cable into the tool and apply firm pressure. Finally, spray liquid electrical tape to any remaining exposed areas and allow this to dry.

What are Amphenol coaxial connectors?

The Amphenol Corporation of New York is one of the world’s largest producers of electrical connectors and related products, with over 45,000 employees in more than 30 countries. Their comprehensive range features thousands of different connectors, including the flat ribbon coaxial connectors widely used for cable TV, audio-visual and telephone equipment.

What are micro connectors?

As the name suggests, micro-coaxial connectors are made for the smallest cables – typically not exceeding 1.5cm in diameter and less than 6 Ghz.Their small size makes them well suited for use in complex but physically small electronics such as mobile phones, GPS receivers, wifi routers, and PC equipment.

What are Radiall connectors?

Radiall is a Paris-based manufacturer of electronic connectors and associated components, working mainly with aerospace, defence, telecommunications and industrial companies around the world.It's extensive product portfolio includes multiple types of radio frequency and coaxial connector.