การค้าหาล่าสุด / Recently searched

    Spotlights & Downlights

    Spotlight and downlights are different forms of lighting typically found in ceilings in kitchens, bathrooms, living rooms and bedrooms. They are integral to providing the required light to a variety of rooms creating the perfect mood setting and enhancing your environment. Spotlights and downlights can add a touch of style and theatre turning an average space into to great space. LED spotlights and LED downlights use LED bulbs which are more energy efficient and do not emit any heat.

    LED downlights

    LED downlights are the perfect lighting solution for any room. They're energy-efficient, and they last for years longer than traditional incandescent bulbs. The LED technology used in each of our LED downlights is designed to provide you with the perfect amount of light for any room in your home, no matter if it's a living room or a kitchen.

    LED spotlights

    LED spotlights are a great way to light up your home or business. They're perfect for highlighting artwork or other important displays, as well as adding ambiance to your living room or dining area. LED spotlights are available in a range of styles and sizes, with some having adjustable heads that allow you to direct the beam of light wherever you need it most.

    What is the difference between downlights and spotlights?

    Downlights and spotlights are both types of lighting fixtures that can be used in residential or commercial spaces. Both types of lighting fixtures are usually used to light up a specific portion of a room, such as a dining table or a kitchen island. The only difference between the two is that downlights are recessed into the ceiling while spotlights are placed on top of the surface they're illuminating.

    Types of finish

    There are many different types of finish available for LED downlights and LED spotlights.

    Matt White

    Matt white is a very popular finish for LED downlights and LED spotlights. It’s an extremely versatile finish that can be used in any type of indoor environment, from commercial projects to residential spaces. Matt white has a sleek, modern look that works well with both contemporary and traditional designs. It’s also one of the most affordable finishes on the market.

    Chrome Satin Nickel

    Chrome satin nickel is another popular choice in the world of LED lights. This finish works well with both modern and traditional designs, making it perfect for use in just about any type of interior setting. The chrome satin nickel finish gives off an elegant appearance that's sure to impress everyone who sees it!

    Antique Brass

    If you want an antique-inspired look for your home or commercial space, then you should definitely consider purchasing antique brass-finished LEDs. These lights give off a warm glow that will instantly transport you back in time! They're also very energy efficient and easy to install.

    Are they easy to install?

    LED downlights

    Yes, they are extremely easy to install. You just need to remove the existing light and screw in the new one. As long as you have a power point nearby, you should be able to do this job yourself without any problems.

    LED spotlights

    As with LED downlights, LED spotlights are also very easy to install. They are usually installed on ceilings or walls, so they require a bit more knowledge than LED downlights, but not much more than that. It all depends on where they are being installed and what kind of fixtures they replace (if any). It's always good to get an electrician if you don't feel confident doing it yourself.

    151 สินค้าที่แสดงสำหรับ Spotlights & Downlights

    ผลลัพธ์ต่อหน้า