การค้าหาล่าสุด / Recently searched

    3M Clear Tapes

    Tapes (also referred to as Adhesive Tapes) are an extremely popular tool in everyday life, whether you need them to seal packages or just to complete your DIY projects, there is no doubt you have at least one type of adhesive tape at home.

    Clear Tapes

    A clear tape is a form of adhesive with a sticky back to them. They benefit from being a clear and transparent tape, making them very versatile for a variety of applications, as they are almost invisible on the surfaces they are applied to.The use of clear tape is endless, ranging from the repairing of paper tears to sealing packages and wrapping presents, to name just a few. Often referred to as office tape, clear tape is commonly found in classrooms and workplaces.The name clear tape is derived from the fact that it is very difficult to see when it is applied in a single layer. There is often a little indication of where the tape is, which is why it is also known as invisible tape. It is a good choice for viewing materials underneath the tape due to the ability to see underneath the tape.The adhesive tape can come in a variety of sizes, with the most common clear tape being 19mm in width.

    Multi-Purpose Clear Tapes

    When gift-wrapping packages at school or in the classroom, it is the first tape most people come across. Tapes of this type usually have a width of about one inch (25 mm). When dispensing disposable tapes, they are often designed with a serrated edge to make it easier for the user to tear off the tape when he or she wants to remove it from the dispenser. There is a level plane just before the serrated edge, which allows the tacky portion to rest, which eases the process of moving on to the next piece.Furthermore, some users may prefer refillable dispensers over throw-away ones. Dispensers that function similarly to throw-away dispensers sit on the desk and are taken with the hand, unlike throw-away dispensers, so that the tape can be discarded. The end of the tape roll can still be rested on the serrated edge of a refillable tape dispenser. You can usually find them in stores that sell the school, desk, or office supplies.Sealing boxes and packages using packaging tape is a common task. The type of clear tape described above is typically not recommended for packing or shipping if harsh conditions are present. Due to its thin width and depth, the tape has a low adhesion rate. The tape, therefore, has a very weak strength. Although this tape may not always be the best choice when packing, particularly when writing an address on the box.It is often possible to resolve this issue by using clear packaging tape. This tape is usually two inches long (50 mm) and has a slightly thicker core than most other kinds. It is therefore very durable and capable of surviving a lot of abuse and use over a long period of time.Let's see some of its core features and benefits.

    Features and benefits:

    The tape can be used to stick multiple pieces of card or paper together at onceCan either be one-sided or double-sided depending on the desired useStrong and long-lastingEasy to cut and manage, and the rolls can fit in an easy-to-use dispenserNo mess or fussWill not damage painted surfacesCan be used for sealing a variety of materials

    คัดกรอง / Filters
    เรียงลำดับตาม
    1 จาก 1
    ผลลัพธ์ต่อหน้า