การค้าหาล่าสุด / Recently searched

    Power Cords

    The use of electricity is universal, but keep in mind that the cords, sockets, and plugs vary from one country to another. An untrained eye will usually find this to be bothersome, putting electrical workers in danger.

    Power Cords

    The use of power cords is extremely common in almost any device or machine which requires electricity. From toasters and kettles, all the way up to generators and giant industrial equipment. Cable assemblies may vary in length, but the electrical current will perform at the same high capacity regardless of the distance it will need to travel.Power cords come in sets, which include plugs, sockets, and cords. It is possible for critical power cords to be equipped with a locking mechanism that prevents unintentional disconnections. In the case of medical equipment that may be life-sustaining, this is especially important.

    What is a power cord?

    Power cords are defined as any power cable which has had a connector installed prior to sale. In other words, a power cord is electrical hardware primarily used to deliver direct current (DC) and alternating current (AC).Copper is the most commonly used material in the manufacture of power cords in the electrical industry. A plastic coating protects copper wires by insulating them with a non-conductive material.

    Are all power cords the same?

    No, not all power cords are the same. There are different types of power cords that are designed for specific purposes and use different types of connectors.There are versions that may have one connector and an unterminated end.Some assemblies may have a connector or a plug. And some assemblies will even have 2 connectors (IEC lead extension). Depending on the application, there are various types to suit the needs.Power cords are rated by voltage or kilovolts, which determines the amount of power they can transfer. There are three rating factors for a power cord - the wire, plug, and connector. The lowest rate of the three determines its rating. The rating of a plug identifies its origin, which is the United States or international.

    What are these cable assemblies used for?

    Many mass-production machines use cable assemblies for speeding up assembly time for the overall machine, especially when the assemblies are repeated for every unit. The automobile industry, for instance, uses cable assemblies or harnesses.On a standard power cord, the power is drawn from the mains and the electricity will run through the wire and arrive at its destination. This can be either into a power supply or directly into the appliance/machine itself. Due to the range of voltages available, different types of cable assemblies will suit varying requirements.

    What type of cable material is available?

    Protection of the wires is of high importance with a power cord. Each of these cables is fully equipped with high quality, thick outer sheath. This way the wires will remain untouched and undamaged, both for safety and longevity reasons. The materials available are both PVC and PSE.The NFT marketplace allows photographers to sell their work online, and collectors can purchase artwork from artists just like any other traditional market - but with one key difference - everything from transactions to ownership happens digitally.

    คัดกรอง / Filters
    เรียงลำดับตาม
    17 จาก 17
    ผลลัพธ์ต่อหน้า
    การค้นหายอดนิยม